Digital Output


What you will find in this section:

  1. Digital output
  2. Related topics

 

The digital output complies with IEC 61131-2 Type 3. It can be configured via the web server or the Modbus communication interface. 

 

Digital output

 

Navigation on the web server

“Settings, Digital output”

 

Menu: “Settings, Digital output”
Menu: “Settings, Digital output”

 

Status

The “Status” area shows the current status of the digital output.

Identifier

The identifier can be used to assign a user-specific designation to the digital output.

Idle level

There are two possible statuses for the idle level.

  • NC: Normally closed
  • NO: Normally open

The default setting for the digital output is NC (normally closed).

Function

Only one function can be configured at a time.

  • Impulse
  • Device status
  • Manual
  • Alarm
  • Rotary field direction
  • BACnet
  • Deactivated

The digital output is deactivated by default.

 

 


EMpro online documentation
Published/reviewed: 2026-07-10, en revision 004, Version history